HI Team,
We tried to use GUI and DRV8899-Q1 to control the motor. It is confirmed that TOOL is connected,
but the motor will not rotate after setting. I want to ask if there is anything that needs attention, thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Team,
We tried to use GUI and DRV8899-Q1 to control the motor. It is confirmed that TOOL is connected,
but the motor will not rotate after setting. I want to ask if there is anything that needs attention, thanks
HI Ryan,
We tried the GUI again to make the motor move, but the motor can only rotate in a single direction.
We choose another direction and it cannot be locked. How can I set the GUI to make it rotate forward and backward, thanks
hi Ryan,
about DRV8899 test, if we want to connect to other MCU,
remove (R3, R4, R6, R7, R9, R11, R12, R14, R15, R16, and R17),
then MCU needs to connect to those points of the DRV8899, To make the MCU and DRV8899 work normally, thank you
HI Ryan,
Because we changed other MCUs to connect with DRV8899, but Motor can’t rotate, please remove (R3, R4, R6, R7, R9, R11, R12, R14, R15, R16, and R17), then when using other MCU, Whether (R3, R4, R6, R7, R9, R11, R12, R14, R15, R16, and R17), also have to be returned, we want to inquire about this, please help confirm, thank you
Removing those resistors physically disconnects the onboard MCU signals from the DRV8899 driver and allows an external MCU to drive the control pins on the DRV8899.
1) How have you connected the external MCU?
2) Have you checked that you have power going to the DRV8899?
3) Have you used a scope to check the STEP input on the device?
4) Are you getting SPI communication between your external MCU and the DRV8899...able to write and read back registers?
5) Have you checked the state of the nFAULT pin on the DRV8899?
6) What is the state of nSLEEP and DRVOFF? nSLEEP should be HIGH and DRVOFF should be LOW.