Part Number: DRV8308
Hi, I've been using this part for a couple years now and I've run into a problem that happens occasionally due to a race condition.
I make use of the 'coast' feature of the device, by bringing the enable line low, on and off pretty often during use. The motor is used in a case where it can be forced to rotate through external forces at any point.
The issue I'm having is that it seems after the enable has been brought low, the motor needs to come to a complete stop before the motor will start up again.
I found this relevant part of the datasheeet:
"8.3.1 RESET and ENABLE Considerations
Since the ENABLE function doubles as a sleep (low-power shutdown) function, there are some important considerations when asserting and deasserting ENABLE and RESET.
While the motor driver is enabled, the deassertion of ENABLE initiates a stop-and-power-down sequence. This sequence starts by disabling the motor (either braking or coasting depending on the BRKMOD bit), and waiting for rotation to stop. After rotation is stopped for 1 s (as determined by the absence of transitions on FGOUT), the internal circuitry is powered-down, the V5 regulator and power switch are disabled, and internal clocks are stopped.
In this low-power sleep state, the serial interface may still be used to read or write registers. All other logic is disabled.
After this stop-and-power-down sequence has been initiated (by deasserting the ENABLE pin for at least 1.2 µs, or by changing the state of the ENPOL bit), the sequence continues to completion, regardless of the state of ENABLE.
If ENABLE is immediately returned to the active state, the motor slows and stops for 1 s, at which point it starts again. If RESET is asserted during power-down (at any time after the deassertion of ENABLE is recognized), it is acted upon when ENABLE is again asserted, and the part powers-up.
If RESET is asserted when ENABLE is active, the motor is stopped similar to the sequence when ENABLE is deasserted. After it is stopped for 1 s, all internal registers are reloaded with the value contained in OTP memory, faults are cleared, and internal states (that is, the speed loop datapath) are initialized. The motor remains disabled until RESET is deasserted.
RESET and ENABLE may be connected together (if the ENPOL bit in OTP memory is programmed so that ENABLE is active low). When both signals are low, the motor is enabled; when both signals are high, the motor is disabled. As soon as the signals are returned to high, all registers are reloaded from OTP memory, faults are cleared, and the motor starts."
I really need the motor to be able to start up even when it is already moving due to outside forces, without ever coming to a complete stop. I also need the motor to be able to completely coast, just setting the speed to 0 through the PWM input still allows the low side FETs to apply a braking force to the motor which I cannot allow.
Any suggestions?