This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2603: Can I drive the DRV2603 from the Lipo 3.7V battery, control the vibration intensity via a microcontroller PWM and EN operating at 1.8V and still obtain a strong vibration intensity for driving my LRA motor?

Part Number: DRV2603
Other Parts Discussed in Thread: DRV2604, DRV2604L

Hello TI Team,

I am using a microcontroller that works at 1.8V.

I have a few questions reg the use of DRV2603 to drive my LRA coin vibration motor.

For my application, I want a strong vibration intensity that can be easily felt on the skin of the user. Also, I want to control the intensity of the vibration (through PWM from a microcontroller). The battery that I am using is a Lipo battery rated at 3.7V and 500 mAH.

My absolutely critical design requirements are: low power, quite strong vibration intensity, vibration intensity should be controllable by microcontroller for providing Low, Moderate and High Vib Intensity levels, smallest possible PCB circuit design for wearable application.

I am exploring some options where I do not have to put additional circuitry for driving the vibration motor, like a Boost converter (5V regulated power supply) or a voltage level shifter to control the DRV2603 through my 1.8V Microcontroller.

Here are my queries:

1. If I drive my DRV2603 circuit by giving 1.8V to the VDD, will the vibration intensity be lesser than if I would drive this IC with a 5V VDD?

2. Supposing if at 5V input power to the DRV2603, the vib motor's vibration intensity is much stronger than the 1.8V input power, then can I give 5V to VDD but still control the ON/ OFF and also vary the vibration intensity through PWM and EN pins that are operating at 1.8V straight from the Microcontroller GPIO (refer to attached picture: Possible Schematic Number 4)? Or would I absolutely have to put a Voltage Logic Shifter between microcontroller and DRV2603 chip and boost the microcontroller GPIO output from 1.8V to 5 V so that the DRV can identify it and allow it to take action (refer to attached picture: Possible Schematic Number 2)?

3. If the answer to my Question 1 is YES, 5V WILL GIVVE STRONGER VIB INTENSITY THAN 1.8V POWER SUPPLY, then If I still want strong vibration intensity while driving the motor at 1.8V, will putting a current amplification buffer circuit at the output terminals of the DRV2603 help?

I have attached a pictorial representation of all my possible schematics herewith. The best possible scenario for me is Schematic No 4 (because I will not have to use a high current buck regulator), if and only if this design can give me very strong vibration intensity.

Request your kind help on the same.

Regards,

Anmol Ajay Saxena