Hi,
I'm trying to move a stepper motor with DRV8811 driver, but i don't understand very well how Vref works...
From Vref i can set Ichop, that represents the peak current in each phase of stepper motor. With
- Vdd=3.3V
- Rsense=0.1ohm
- Ichop=900mA
i obtain Vref=0.72V. During motor movimentation, i see (from power supply)
- current varies with Vmotor
- at 24V current isn't 900mA, but 0.2A
What's the problem?
Thanks