Hi
I'm new to the DRV8811 and have a first proto board up and running driving two small-ish hybrid steppers connected in series bipolar fashion. They are 8-wire types with 1amp 5V phase windings (each of the 4). So in series they are "10V 1amp".
They step OK after a bit of fooling around. But they squeel and hiss all the time (like boiling kettles!). The two driver chips are medium warm, not "hot" in my estimaiotn. I can affect the hissing (and chip temp) by adjusting the current setting via a multi-turn pot controlling Vref level.
I have 30K and 1nF for the time constant components (was 47K and 1nF but reading some other threads prompted the move to a little higher chopping frequency).
In full step mode I *can* make them quiet, setting Vref to around 1.35V (Vdd is 3.3V). I use 0.2ohm sense resistors and Vmot is 12V. But they seem to be on the edge of non-operating when at this quiet point. In micro step mode they are always noisey regardless of the pot (the squeeling just changes its fundamental frequency). They do step OK in microstep btw.
So I'm a bit puzzled what to try next. I'm using sync rectification btw.
TIA