This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8829: OUTx shorted to GND.

Guru 11175 points
Part Number: DRV8829

Hi team,

The resistance value of the OUTpin to GND was 0.1Ω.
I think the Lowside FET seems to be broken.
What are the factors that cause the Lowside FET to break?
What is the current rating of the Lowside FET?

Sincerely.
Kengo.

  • Hi Kengo,

    Exceeding the maximum current, temperature,and voltage specifications of the device for a prolong time can damage the FETs. Isolated events like ESD or large voltage/current spikes in the system can also damage the device.

    The DRV8829 device can drive up to 5-A continuously with thermal and power dissipation being a limiting factor.