This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8912-Q1: limitations power with solenoid

Part Number: DRV8912-Q1


hi, i have problems in my prototipe when i tried to open a solenoid, when the VM is between 8-18V i dont have problems, but if upper the voltage VM to 24V the solenoid doenst works and status said that i have overcurrent. the maximun current output by channel is 1A. ¿is it possible leave the proteccion overcurrent (OCP)? only i need open solenoid for 150ms or close for the same time and only open 2 times day.

i dont strees the solenoid when it is installed in the field.

the solenoid´s power is high when the voltage ups. maybe is the reason of overcurrent. is there some secret adress to change OCP on-off?

is posiblle solve this? i know that i can used more pararell channels and open but the idea is has 10 solenoids, and open close sequencial, never same time.

thank you.