Hello Guys,
Good day.
Our customer seems to found an error on equation1 page26 of the datasheet. Calculating I(CHOP) using the sampled data gives 2.33A not 3.28 as suggested on the datasheet. Is that an error?
(3.3-(0.05*19.8))/(19,8*0,05)=2.33A
Another issue is, if he calculate with the same data as before the H-bridge current (7.3.5 Amplifier Output), he gets only 1.31A from the equation, where he calculate the Vso parameter with the previous calculated Chopping current .
But here comes another question: If you want to calculate the H-bridge Current from Vso parameter that depends from the bridge current, the equation is recursive. (Vso=Rsense*Ibridge*19.8) It can be normal, that the bridge current is weaker than the chopping current, but if he use 0.005Ohm current sense resistor, instead of 0.05Ohm, he get for I chop 23.3A, and for Ibridge -7.69A! How can the bridge current be negative?
Would appreciate it where do you think he got it wrong, and step for step the calculations sequence.
Circuit parameters:
Device= DRV8702-Q1
Mode=HiZ
Vref=AVDD
VDS=HiZ
Idrive=220KOhm to GND
Bridge current must be 12A
Overcurrent can be 12A-15A
Thanks in advance!
Art