I am working on a project involving manually commutating a stepper using the DRV8434PRGER, while still driving VREFA and VREFB sinusoidally to microstep with Smart Tune Ripple Control enabled. My understanding would suggest that I should control current direction for each H-bridge with AIN1 and BIN1 (imagining that they're driving the left side of each H-bridge), and that if I wanted to manually chop for current control I would control AIN2 and BIN2 (imagining that they're driving the right side of the H-bridge). Given that I want to control current with VREFA and VREFB, it seems that either xIN1 or xIN2 should be left un-driven for my application, and that the IC would do this chopping for me. Do I need to configure the IC in any way for this? Is there a preference for controlling current direction with either xIN1 or xIN2?
The relevant header in the datasheet for Table 7-3. DRV8434P (PWM) Control Interface says "Note that this table does not take into account the current control built into the DRV8434P." From what I can tell the datasheet does not specify which pair of FETs are driven by the decay mode.