This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305: Tying the Vreg pin to external source

Part Number: DRV8305
Other Parts Discussed in Thread: LMR36015-Q1, , LMR36015

Originally a DRV8305N was used on a board design but it got switched to a DRV83053 variant. 

The Vreg pin (outputs 3.3V from the DRV internal LDO) is connected to our boards switching regulator (LMR36015-Q1).

The question here is will this connection of the outputs of the 2 regulators affect the motor control performance of the DRV8305 in any way 
One of our chief concerns is how/if this will change with temperature variance