Other Parts Discussed in Thread: DRV8662
Hello team,
I use the DRV8662EVM to output a ±100V signal. When I choose the External Analog Input Mode, the external input signal I use is a 250Hz 1.8Vpp sine wave and when I choose External PWM Input Mode the input signal is a 10KHz 1.8Vp PWM wave. But both of them cannot achieve ±100V, so
1. Where is the problem?
2. What are your suggest signal when I choose External Analog Input Mode and External PWM Input Mode?
Best wishes,
Boyuan Huang