This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605LEVM-MD: How to set the output of OUT5 and OUT6 at the same time when pressing the B1 button

Part Number: DRV2605LEVM-MD


Hi

1;How to set the output of OUT5 and OUT6 at the same time when pressing the B1 button

2: When pressing B1 button, how to set the output time of OUT5 and OUT6

3: When the B1 button is pressed, whether the output waveform of OUT5 and OUT6 can be changed

4: Press the B1 button to control only OUT5 and OUT6 output ports. The output time of the ports can be adjusted. Is the waveform adjustable

thanks!

  • Hello Neal, 

    You can control the outputs individually using the Haptics Control Console GUI. This allows you to choose which outputs are active and change the waveform that is played on those outputs. Putting the EVM in USB mode does remove the capacitive button functionality though so you would then need to use the GUI to start the outputs. 

    Best Regards, 

    Justin Beigel