Hi,
We are making a BLDC driver with DRV8306 that will fit into the motor itself. Thus, we are a bit constrained on how much space we can use. The tallest component is the 220uF decoupling capacitor at the power input. We were wondering if there was a way to find the optimal value of the capacitor (apart from trial and error) as having a smaller value decoupling capacitor will reduce the space we require within the motor.