Hi Team,
The customer asked questions when connecting MCU to DRV8316.
It's a 5V MCU.
Question
Q1. The AVDD output voltage value is 3.3V, should the VREF be used as a 2.8V to 3.3V input?
Q2. Is the VREF value 5V value available?
Q3. If I don't use the BUCK function, do I just need to disable the PIN NC & BUCK_SEL bit?
* Delete Attachment