Hello,
I'm looking through TI's motor drive/haptic driver portfolios for a device to replace a MAX1749 vibrator motor driver.
I found the DRV8601 to be a decent replacement but was wondering if there are any other similar TI haptic drivers that would perform the same function but without the need for a PWM input or other communication interface (SPI, I2C, SMBus, etc..). The MAX1749 is activated with a single ON/OFF enable pin.
Thank you