We are having an issue integrating our DRV8343 in a 3phase BLDC motor configuration.
We have now had two instances where we believe we have our software configuration set up, we are able to drive each Phase individually with a resistive load, and the High Side and Low Side seem to be functioning properly. However, when we go to actually try driving a 3 Phase Motor with hall-effect/state feedbacks we somehow have managed to blow the chip.
After reviewing the power stage circuit from the DRV8343X-Q1EVM schematics (MD005A(001)) I noticed that there is a 330uF Capacitor in parallel with a 1uF and 10nF capacitor. We do not currently have a capacitor on the Drain of the High Side of the power stage FETs. Would you expect that there would be some sort of inductive feedback from the motor that would cause a feedback into the DRV8343 that could damage it without the presence of this large electrolytic (330uF)? That looks to be the only difference between our design and the evaluation board so I'm just wanting to know if perhaps there is something else I may be missing with our setup.
Also, we do have a main power relay architecture that self protects (turns off VM) when there is an over-voltage condition of 36V or greater. If this turned off because there was a load dump/transient spike, could this be a potential cause of VM trying to find a return path through the DRV8343.
Thanks in advance.