This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8350R: Can dvr8350R used to drive the CSD18532KCS 60V N channel MOSFET?

Part Number: DRV8350R
Other Parts Discussed in Thread: CSD18532KCS, DRV8350, , CSD19532Q5B

Can  dvr8350R   used to drive the CSD18532KCS 60V N channel  MOSFET? 

I have referenced the DRV8350 evm, It use the drv8350R  to drive the csd19532q5b, I have found the Rds(on) are almost same, also, the Vgs are same.

So if I can confirm that the DRV8350  can also used to drive the CSD18532KCS 60V N channel  MOSFET with no schematic change?

Waiting for your answer.

Thank you !