Other Parts Discussed in Thread: DRV8304
Hi,
I have a question, in datasheet from DRV8343 there is the following text,
In 3x PWM mode, the INHx pin controls each half-bridge and supports two output states: low or high. The INLx
pin is used to put the half bridge in the Hi-Z state. If the Hi-Z state is not required, tie all INLx pins to logic high.
In DRV8304 does not exist the same information but the PWM 3X mode is supported too. So I made a test with drv8304 and it seems to working.
Is it correct? Can I use this also with DRV8304 so I need only 3 PWM Channels?
King Regards,
Nikos