Hi Team,
Customer use the following parameters here, and a continuous and complete PWM waveform can be measured at AOUT1 of the EVM.
But under the same conditions, I have measured incomplete waveforms on our PCB (please see the picture below). What conditions can cause this phenomenon
Motor parameter:
Full Step
Frequence:600Hz
PPS:300
Torque_DAC:5% / 41mA
Winding resistance : 215ohm +-7%/phase