Part Number: DRV8343-Q1
Hi Team,
My customer has a question regarding DRV8343-q1 in their motor board. They are getting an interesting output waveform on the SOA, SOB, SOC outputs. A shot of the waveform is attached along with schematic pages of the motor power stage and controller. We checked the current through the motor phases and the waveform looks normal, so only at the SOx output is it acting strange. The register commands are written below:
Register: Command
0x05: 0x40
0x06: 0xCC
0x07: 0xCC
0x08: 0xCC
0x09: 0x99
0x0A: 0x99
0x0B: 0x99
0x0C: 0x2C
0x0D: 0x61
0x0E: 0x00
0x0F: 0x15
0x10: 0x3F
0x11: 0x00
0x12: 0x00

Thanks,
Mitchell