Other Parts Discussed in Thread: DRV10983, USB2ANY
I tried all the suggestions in the thread previously on this, with no luck. I still get the following message: "
Register.vi<ERR>
Register reading not successful!! Please restart the GUI and try again"
Notes:
1. DRV10983 is NOT in sleep mode- I see the switcher switching with a scope, and 5V is present.
2. I un-installed the GUI and USB2ANY and created a new directory with correct permissions, and re-installed them there.
3. I am applying 12.0 V to the EVM, it is drawing around 6mA.
4. Running Windows 10, 64 bit.
5. I can make my motor run by turning the pot, so the DRV10983 is clearly okay. Just the GUI does not seem to be able to communicate with it.