Other Parts Discussed in Thread: DRV8848, DRV8847, DRV8848EVM
Hi All
Currently I am using TB6612FNG Motor Driver for my commercial project (Line follower robot) .It has two motors
All power consumption below 10W
I need little higher performance Motor Driver better that TB6612FNG
The size of the motor driver should almost same as TB6612FNG
Motor Specification
No-load speed @ 12V: 650 rpm
No-load current @ 12V: 0.06 A
Stall current @ 12V: 0.75 A
Max output power @ 12V: 1.1 W
Note
Also I suppose to use 6v motors with project
Please advice
Thanks in advanced