Part Number: DRV8825
Other Parts Discussed in Thread: DRV8424
Hi Sir
I use GPIO to change xVref voltage and IFS current
TB_HOLD=H current is 349.7mA
TB_HOLD=L current is 773.8mA
When I change TB_HOLD from low to high ,but the current still keep 773.8mA
Have anything need to take care ?
PS. When I set xVref voltage up to 1V,the issue is still exist
This issue only happen on mixed decay mode , fast decay mode is workable
Yellow is TB_HOLD
Green is DIR
Red is output current
below figure is abnormal ,should be 349.7mA (H) not 773.8mA