Hello Rakesh,
Can you recommend a 10" multi-touch display that would connect to HDMI or 100-pin port ? Please also explain the setup of multi-touch, where it is connected and if there is a driver in the Linux SW package.
Thanks a lot !
Alexey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rakesh,
Can you recommend a 10" multi-touch display that would connect to HDMI or 100-pin port ? Please also explain the setup of multi-touch, where it is connected and if there is a driver in the Linux SW package.
Thanks a lot !
Alexey
Hi Alexey,
Below is the information for Multi-Touch Display support on OMAP5432-EVM,
Please contact the partners if you need support for this feature.
Hi Peng,
Please conatct our recommended scaling partners for further support on this issue.
Hi M F,
What's the connection between your Lilliput 7" touch screen and OMAP5EVM? HDMI?
I also hope can get some information to buy the Multi touch display for OMAP5EVM. I talked with SVT, they said they are working on this.
Thanks,
-Peng
I am able to make the Acer T232HL which is an HDMI with touch screen to work with the omap5432 uEVM. get the patch from the below site
https://chromium-review.googlesource.com/#/c/39576/2
then down load the new zImage. One more thing don't use the usb cable that comes with the monitor use a normal usb without the extra connector.
When you boot the board don't connect the USB cable from the touch screen. Once Android boots then you can connect the touch screen usb cable.
Also for some reason or other i can't get the multitouch to work. Once i get it working i will let you know.
Good luck let me know if you need nay help with this.
Regards
Mohsen