Hello,
I would like to ask if there is TI software for OMAP5 that accelerates OpenCV code (using e.g. the DSP features and the floating point unit).
I want to use OMAP5 to a accelerate a computer vision algorithm for a linux embedded application.
The computer vision algorith will execute convolutions and matrix operations.
If this software exists, I would also like to know about the following:
- which linux kernel must I use - is there a specific TI linux kernel for the OMAP5432 Processor-based EVM that supports the computer vision acceleration software?
- which linux distributions that can be used with this specific kernel?
- what are the OMAP5 software tools that are available for accelerating a computer vision algorithm and match that specific kernel - is there a software tools that supports OpenCV that takes advantage of the DSP features and floating point unit of OMAP5?
If there is any OMAP5 software tools that can be used for accelerating (DSP+hard floating point unit usage) a computer vision algorithm (convolutions and matrix operations) on the OMAP5432 Processor-based EVM, please be kind to provide to me the relevant information.
Thanks in advance,
Panayiotis Mousouliotis