Other Parts Discussed in Thread: DRA742
Dear Team,
I got an opportunity to work with Jacinto6 evm board, model: TI DRA742, and want to test the board with enabling the CAN into it.
I am using the following s/w packages :
Kernel Linux 3.8.13
OS Android KitKat 4.4.2
Toolchain Andriod linux-x86 toolchain arm-eabi-4.7
I tried to flash the board with pre-built image as well as my customize kernel image(by enabling "Generic Platform Bus based C_CAN/D_CAN driver" at networking support module in kernel), but getting stuck at finding the output at CAN analyser tool, as I am not able to identify how to use CAN1, DCAN1 and DCAN2 pins on the board.
It will be appreciable if you can provide me the detailed board specs or the useful links for the board on subject matter as you have provided for AM335X board.
Thanks you,
Rohit