Other Parts Discussed in Thread: DRA752
Hello,
We are working on dra7xx-evm(OMAP5777) board. Here we are using these things:
1. linux3.8
2. Toolchain- gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux.
3. Filesystem- arago-glsdk-multimedia-image-dra7xx-evm.
We are trying to run sample application kmscube to test display on dra7xx-evm. But we are not getting any display.
We are getting the following log while running kmscube app given in filesystem.
The log :
root@dra7xx-evm:~# kmscube
trying to load module omapdrm...success.
### Display [0]: CRTC = 10, Connector = 4
Mode chosen [800x480] : Clock => 29232, Vertical refresh => 60, Type => 72
Horizontal => 800, 841, 890, 931, 0
Vertical => 480, 493, 497, 526, 0
### Primary display => ConnectorId = 4, Resolution = 800x480
failed to load module: /usr/lib/gbm/gbm_dri.so: cannot open shared object file: No such file or directory
failed to load module: /usr/lib/gbm/gbm_gallium_drm.so: cannot open shared object file: No such file or directory
loaded module: gbm_pvr.so
PVR:(Warning): PVRSRVOpenDCDevice: Warning - 138 returned [80, /bridged_pvr_dc_glue.c]
Using display 0x1 with EGL version 1.4
EGL Version "1.4 build 1.9@2253347"
EGL Vendor "Imagination Technologies"
EGL Extensions "EGL_IMG_client_api_ogl EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cu"
Please help in this regard.
Regards
Naveen