Hello E2E Experts,
Good day.
We are using the TPS5432 regulator in our design. If we give a sudden load for 1A it starts generating a sine wave as output?
I connected the regulator output side with 100mA constant load, then I suddenly added 850mA load parallels to 100mA load. after adding this it started sine wave.
Attached is a scope and schematic.


Using the same regulator we have designed for 1.2V and 1.8V too, the same issues we found on those too.
scenario 2: When we provided a 100mA constant load from the beginning itself, it is the same as in the scenario1, but when I'm changed the load suddenly to 1A or suddenly disconnect the 1A load from the circuit, it started to oscillate like an AC sine wave, at the same time I checked the PH pin switching signal it is different from the scenario 1. we noticed an unusual switching on it. The scope images are attached for your reference. The output voltage level's also changed, they started varying and it did not attain its stable state. When I disconnect DC power and reconnect it becomes stable.
The circuit we used in our design was taken from TI's Webench circuit simulator.
I have attached more scope images for your reference.