Part Number: TPS2552
Other Parts Discussed in Thread: TPS25221
Hello team,
i received some questions from my customer about the enable behavior and its threshold variation of TPS2552. I would appreciate if you could give us an advice about it.
(1) The OUT pin output appears to be disabled when the pin has a momentary H-level applied even if its not a continuous H-level. Is this behavior normal?
(2) The variation in the limit current value seems to appears in IOS min <- IOS nom -> IOS max, but what is the main cause of the variation?
Ambient temperature? Tj? Or is it the Variation between each device?
(3) What should we do to reduce this variation? (ideally zero) Are there any devices that have a similar functions other than the TPS2552 without a variation?
(4) Are there any recommended devices other than the TPS2552 with a similar function?
(5) If there is a variation between each device, we want to know the quantitative evaluation criteria such as the distribution.
Best Regards,
Ryotaro Fukui