Part Number: BQ25798
Other Parts Discussed in Thread: BQ76942, , , BQ76942EVM, TPS61200
Hello,
I'm looking for confirmation & advice on using BQ25798 & BQ76942 to manage power flow between a 2S2P solar input delivering 4.5--5.5V at <1A into the BQ25798 and charging a 4S or larger set of batteries via the BQ76942. Out of the BQ25798's SYS output, we'll deliver an expected 12--15V to a PMIC.
Given the newness of these two BQ components, there's not much information yet available. I'm hoping for some basic confirmation as to if this is likely to be a workable solution and if not, for suggestions on alternatives.
Thank you!