Other Parts Discussed in Thread: TPS55288
I think of using one of the TPS552882 parts for a solar panel powered system. The characteristics of the system is:
- Solar voltage panel 50W, maxpower at 17.2Volt and 2.91Amp
- The destination of the power is a battery of supercaps, 10F and 15Voltmax
- I expect input voltage to vary from a few volts to max 25Volt and the available input current from almost zero to 3.25Amp
- I expect the supercap battery voltage to vary from below 5Volt to max 15Volt (or possibly 18Volt if I add one more cell)
- I have a separate circuit for balancing the super caps such that the battery appears as one single capacitor
Because the input power will vary with weather conditions and the supercap battery does not have a constant voltage and also have a much larger capapacity value than the Cout value in the datasheet I would like to somehow use the converter as a current source rather than as a voltage source.
I have a separate controller and algorithm for adjusting the power drawn from the solar panel in such a way, that the solar panel will always be loaded close to the maximum power point. This algorithm relies on the ability to control how much power the converter draws.
My questions comes down to these:
- Can TPS552882 be operated in a stable mode when loaded by 10F?
- Can the ILIM input be used to control the output current from TPS552882 by connecting a controlled current sink to the terminal instead of R6?
- Can the output current be regulated all the way down to zero (or close)?
- Can you suggest other ways to use TPS552882 as a controlled current source?
Kind Regards
Per Gaarde-Nissen
Senior R&D
Khepri