Could you please provide a reference design for the control loop design using TPS54A20?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The product folder has reference designs.
Hi David, thanks for your quick response. I check all documents and cannot find the application notes for the control loop design. The closing thing I get is the PMP15008 Test Report. It demonstrates the reference design meets the specs of Output voltage deviation is within ±2% of the output voltage when 5 A load steps with 1 A/µs slew rate.
How the control loop is designed to meet these specs? Is there anything else the customers should be aware of in the control design?
Thanks
The control loop is proprietary and not discussed in public forums.
Customers follow the design procedure in the datasheet or use webench to determine the external components.
webench or pspice simulations can verify the performance.
I am searching for the engineer with the small signal models and simplis model and will get back with you