Other Parts Discussed in Thread: LMR33640,
Hello, the LMR33630 is not available anywhere that we've seen; can we use the LMR33640 instead?
Thanks,
Derek
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Derek,
The LMR33640 is the 4A version and is pin to pin compatible with the LMR33630. You should be able to simply drop in place this device and all should work fine assuming that you are using the DDA (HSOIC) package.
Regards,
Jimmy