Other Parts Discussed in Thread: BQ24715, BQ40Z50
Dear experts,
I am designing a battery management system based on BQ40Z50-R2 as a battery monitor and BQ24715 as a smart charger. There are no EC in the system, only the monitor and the charger, which communicate via SMBus broadcasts. My batteries are 3S5P NCR18650B. The charging works OK, except for it can't be properly terminated.
Based on NCR18650B datasheet, I set the termination current to 325 mA (65x5 mA). However, the charging suddenly stops when current goes down to approx. 700 mA in CV phase. No protections or flags are triggered. The boards are barely warm. There's also no specific broadcast from BQ40Z50 that could tell the charger to stop. The watchdog timeout isn't expired.
Don't know where else to look. The charging log and gg.csv files are attached below.
Best regards,
Michael
Wed May 05 22:36:21 MSK 2021 Device Name = bq40z50R2 Firmware Version = V2_08_BLD0050 Design Capacity = 16750 Design Voltage = 10800 Specification Info = 0x0031 Manufacturer Date = 2020-10-18 Serial Number = 0xFBFE Manufacturer Name = Texas Instrument Device Name = bq40z50-R2 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,MaxTurboPwr,SusTurboPwr,MaxTurboCurr,SusTurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,GaugeTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,RawDOD_3,RawDOD_4,CBTime1,CBTime2,CBTime3,CBTime4,CBDOD_1,CBDOD_2,CBDOD_3,CBDOD_4,CBTotalDODChg,SOH_FC_Q,SOH_FC_E,LogRowTime(ms),LogStatus 1,2021-05-05 22:36:25,4.004,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12578,1631,1715,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15719,-15719,-18713,-18713,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4193,4190,0,12571,12675,1616,1620,1613,0,678,679,676,0,2046,2149,29.4,25.2,25.9,25.7,196.1,25.9,-273.2,25.6,6388,6808,6276,6670,6512,6388,6808,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,244,576,512,576,0,-155,-191,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-155,1,0.42,4065,576,512,576,0,282,1140,0,0,576,512,576,0,16384,5836,5924,1265,SUCCESS 2,2021-05-05 22:36:29,8.002,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12576,1544,1689,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15722,-15722,-18717,-18717,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4193,4190,0,12570,12672,1560,1546,1571,0,654,648,658,0,1947,2112,29.4,25.2,25.9,25.7,195.6,25.9,-273.2,25.6,6390,6810,6276,6670,6514,6390,6810,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,248,576,512,576,0,-157,-193,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-157,1,0.42,4065,576,512,576,0,282,1136,0,0,576,512,576,0,16384,5836,5924,1137,SUCCESS 3,2021-05-05 22:36:33,12.002,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12575,1542,1655,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15731,-15731,-18727,-18727,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4193,4190,0,12570,12673,1535,1546,1549,0,644,648,649,0,1948,2072,29.4,25.2,25.9,25.7,196.3,25.9,-273.2,25.6,6392,6812,6276,6670,6516,6392,6812,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,252,576,512,576,0,-159,-195,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-159,1,0.42,4065,576,512,576,0,282,1132,0,0,576,512,576,0,16384,5836,5924,1146,SUCCESS 4,2021-05-05 22:36:37,16.002,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12578,1553,1630,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15742,-15742,-18740,-18740,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4193,4190,0,12569,12673,1533,1527,1530,0,643,640,641,0,1943,2043,29.4,25.2,25.9,25.8,195.2,25.9,-273.2,25.6,6393,6814,6276,6670,6517,6393,6814,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,256,576,512,576,0,-160,-197,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-160,1,0.42,4065,576,512,576,0,282,1128,0,0,576,512,576,0,16384,5836,5924,1155,SUCCESS 5,2021-05-05 22:36:41,20.002,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12580,1522,1608,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15738,-15738,-18736,-18736,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4193,4189,0,12569,12674,1503,1493,1507,0,630,626,631,0,1909,2015,29.5,25.2,25.9,25.8,196.1,25.9,-273.2,25.6,6395,6816,6276,6670,6519,6395,6816,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,260,576,512,576,0,-162,-199,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-162,1,0.42,4065,576,512,576,0,282,1124,0,0,576,512,576,0,16384,5836,5924,1242,SUCCESS 6,2021-05-05 22:36:45,24.003,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12576,1497,1583,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15750,-15750,-18750,-18750,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4193,4189,0,12570,12673,1479,1478,1465,0,620,620,614,0,1876,1983,29.5,25.2,26.0,25.8,196.3,26.0,-273.2,25.6,6397,6819,6276,6670,6521,6397,6819,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,264,576,512,576,0,-164,-202,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-164,1,0.42,4065,576,512,576,0,282,1120,0,0,576,512,576,0,16384,5836,5924,1171,SUCCESS 7,2021-05-05 22:36:49,28.003,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12577,1484,1556,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15746,-15746,-18745,-18745,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4193,4190,0,12569,12673,1468,1465,1461,0,615,614,612,0,1860,1951,29.5,25.2,25.9,25.8,196.3,25.9,-273.2,25.6,6398,6820,6276,6670,6522,6398,6820,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,268,576,512,576,0,-165,-203,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-165,1,0.42,4065,576,512,576,0,282,1116,0,0,576,512,576,0,16384,5836,5924,1119,SUCCESS 8,2021-05-05 22:36:53,32.003,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12576,1444,1534,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15746,-15746,-18745,-18745,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4193,4189,0,12569,12674,1432,1434,1434,0,600,601,601,0,1818,1922,29.5,25.3,25.9,25.8,196.1,25.9,-273.2,25.6,6400,6822,6276,6670,6524,6400,6822,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,272,576,512,576,0,-167,-205,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-167,1,0.42,4065,576,512,576,0,282,1112,0,0,576,512,576,0,16384,5836,5924,1175,SUCCESS 9,2021-05-05 22:36:57,36.003,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12578,1437,1512,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15754,-15754,-18755,-18755,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4191,4194,4189,0,12570,12672,1416,1414,1431,0,593,593,599,0,1806,1895,29.5,25.3,25.9,25.8,196.1,26.0,-273.2,25.7,6402,6825,6276,6670,6526,6402,6825,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,276,576,512,576,0,-169,-208,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-169,1,0.42,4065,576,512,576,0,282,1108,0,0,576,512,576,0,16384,5836,5924,1153,SUCCESS 10,2021-05-05 22:37:01,40.003,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12577,1428,1495,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15766,-15766,-18769,-18769,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4193,4189,0,12569,12673,1404,1398,1397,0,589,586,585,0,1780,1873,29.5,25.3,25.9,25.8,196.3,25.9,-273.2,25.6,6403,6826,6276,6670,6527,6403,6826,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,280,576,512,576,0,-170,-209,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-170,1,0.42,4065,576,512,576,0,282,1104,0,0,576,512,576,0,16384,5836,5924,1193,SUCCESS 11,2021-05-05 22:37:05,44.004,0x0187,300,10,0x0081,0,65535,65535,1,25.9,12578,1418,1475,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15766,-15766,-18769,-18769,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12570,12674,1401,1405,1400,0,587,589,587,0,1785,1851,29.6,25.3,26.0,25.8,195.7,25.9,-273.2,25.6,6405,6829,6276,6670,6529,6405,6829,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,284,576,512,576,0,-172,-212,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-172,1,0.42,4065,576,512,576,0,282,1100,0,0,576,512,576,0,16384,5836,5924,1123,SUCCESS 12,2021-05-05 22:37:09,48.004,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12579,1411,1461,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15778,-15778,-18783,-18783,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4194,4190,0,12572,12674,1402,1398,1381,0,588,586,579,0,1776,1833,29.6,25.3,25.9,25.8,196.1,25.9,-273.2,25.6,6406,6830,6276,6670,6530,6406,6830,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,288,576,512,576,0,-173,-213,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-173,1,0.42,4065,576,512,576,0,282,1096,0,0,576,512,576,0,16384,5836,5924,1132,SUCCESS 13,2021-05-05 22:37:13,52.004,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12578,1402,1449,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15778,-15778,-18783,-18783,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12571,12675,1377,1380,1373,0,577,579,575,0,1762,1818,29.6,25.3,25.9,25.8,196.1,25.9,-273.2,25.6,6408,6832,6276,6670,6532,6408,6832,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,292,576,512,576,0,-175,-215,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-175,1,0.42,4065,576,512,576,0,282,1092,0,0,576,512,576,0,16384,5836,5924,1174,SUCCESS 14,2021-05-05 22:37:17,56.004,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12578,1387,1436,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15781,-15781,-18787,-18787,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12572,12675,1375,1366,1365,0,577,573,572,0,1738,1802,29.6,25.3,26.0,25.9,196.3,26.0,-273.2,25.7,6409,6833,6276,6670,6533,6409,6833,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,296,576,512,576,0,-176,-216,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-176,1,0.42,4065,576,512,576,0,282,1088,0,0,576,512,576,0,16384,5836,5924,1152,SUCCESS 15,2021-05-05 22:37:21,60.005,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12577,1361,1420,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15785,-15785,-18792,-18792,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12571,12674,1327,1319,1330,0,556,553,557,0,1699,1781,29.6,25.3,26.0,25.8,197.6,26.0,-273.2,25.7,6411,6836,6276,6670,6535,6411,6836,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,300,576,512,576,0,-178,-219,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-178,1,0.42,4065,576,512,576,0,282,1084,0,0,576,512,576,0,16384,5836,5924,1160,SUCCESS 16,2021-05-05 22:37:25,64.005,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12578,1333,1399,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15790,-15790,-18798,-18798,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12572,12675,1312,1312,1311,0,550,550,549,0,1677,1753,29.6,25.3,26.0,25.9,196.1,26.0,-273.2,25.7,6412,6837,6276,6670,6536,6412,6837,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,304,576,512,576,0,-179,-220,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-179,1,0.42,4065,576,512,576,0,282,1080,0,0,576,512,576,0,16384,5836,5924,1122,SUCCESS 17,2021-05-05 22:37:29,68.005,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12579,1319,1380,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15797,-15797,-18806,-18806,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4194,4190,0,12573,12674,1295,1302,1284,0,543,546,538,0,1654,1731,29.7,25.3,26.0,25.9,196.1,26.0,-273.2,25.7,6414,6840,6276,6670,6538,6414,6840,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,308,576,512,576,0,-181,-223,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-181,1,0.42,4065,576,512,576,0,282,1076,0,0,576,512,576,0,16384,5836,5924,1146,SUCCESS 18,2021-05-05 22:37:33,72.005,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12578,1304,1363,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15793,-15793,-18801,-18801,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12571,12675,1278,1286,1297,0,536,539,543,0,1644,1709,29.7,25.3,26.0,25.9,196.3,26.0,-273.2,25.7,6415,6841,6276,6670,6539,6415,6841,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,312,576,512,576,0,-182,-224,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-182,1,0.42,4065,576,512,576,0,282,1072,0,0,576,512,576,0,16384,5836,5924,1140,SUCCESS 19,2021-05-05 22:37:37,76.006,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12577,1269,1344,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15801,-15801,-18811,-18811,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4191,4194,4190,0,12572,12674,1247,1242,1253,0,523,521,525,0,1589,1684,29.7,25.3,26.0,25.9,195.0,26.0,-273.2,25.7,6417,6843,6276,6670,6541,6417,6843,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,316,576,512,576,0,-184,-226,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-184,1,0.42,4065,576,512,576,0,282,1068,0,0,576,512,576,0,16384,5836,5924,1210,SUCCESS 20,2021-05-05 22:37:41,80.006,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12576,1220,1320,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15805,-15805,-18815,-18815,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4194,4189,0,12570,12672,1203,1196,1202,0,504,502,504,0,1530,1651,29.7,25.3,26.0,25.9,196.1,26.0,-273.2,25.7,6418,6845,6276,6670,6542,6418,6845,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,320,576,512,576,0,-185,-228,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-185,1,0.42,4065,576,512,576,0,282,1064,0,0,576,512,576,0,16384,5836,5924,1110,SUCCESS 21,2021-05-05 22:37:45,84.006,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12576,1212,1295,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15813,-15813,-18825,-18825,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4194,4190,0,12570,12672,1190,1194,1196,0,499,501,501,0,1520,1621,29.7,25.3,26.0,25.9,196.1,26.0,-273.2,25.7,6419,6846,6276,6670,6543,6419,6846,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,324,576,512,576,0,-186,-229,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-186,1,0.42,4065,576,512,576,0,282,1060,0,0,576,512,576,0,16384,5836,5924,1104,SUCCESS 22,2021-05-05 22:37:49,88.006,0x0187,300,10,0x0081,0,65535,65535,1,26.0,12575,1193,1272,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15813,-15813,-18825,-18825,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12570,12673,1172,1170,1162,0,491,491,487,0,1500,1593,29.7,25.3,26.0,25.9,196.1,26.0,-273.2,25.7,6421,6848,6276,6670,6545,6421,6848,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,328,576,512,576,0,-188,-231,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-188,1,0.42,4065,576,512,576,0,282,1056,0,0,576,512,576,0,16384,5836,5924,1162,SUCCESS 23,2021-05-05 22:37:53,92.007,0x0187,300,10,0x0081,0,65535,65535,1,26.1,12577,1187,1253,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15821,-15821,-18835,-18835,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12570,12673,1161,1172,1168,0,487,492,489,0,1490,1570,29.8,25.3,26.1,25.9,196.1,26.1,-273.2,25.7,6422,6849,6276,6670,6546,6422,6849,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,332,576,512,576,0,-189,-232,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-189,1,0.42,4065,576,512,576,0,282,1052,0,0,576,512,576,0,16384,5836,5924,1123,SUCCESS 24,2021-05-05 22:37:57,96.007,0x0187,300,10,0x0081,0,65535,65535,1,26.1,12576,1173,1235,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15825,-15825,-18839,-18839,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4194,4190,0,12571,12672,1154,1141,1168,0,484,479,489,0,1470,1548,29.7,25.3,26.1,25.9,196.3,26.1,-273.2,25.7,6423,6851,6276,6670,6547,6423,6851,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,336,576,512,576,0,-190,-234,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-190,1,0.42,4065,576,512,576,0,282,1048,0,0,576,512,576,0,16384,5836,5924,1131,SUCCESS 25,2021-05-05 22:38:01,100.007,0x0187,300,10,0x0081,0,65535,65535,1,26.1,12576,1157,1218,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15821,-15821,-18835,-18835,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4194,4190,0,12570,12672,1151,1136,1144,0,482,476,479,0,1454,1526,29.7,25.3,26.0,25.9,196.3,26.0,-273.2,25.7,6425,6853,6276,6670,6549,6425,6853,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,340,576,512,576,0,-192,-236,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-192,1,0.42,4065,576,512,576,0,282,1044,0,0,576,512,576,0,16384,5836,5924,1109,SUCCESS 26,2021-05-05 22:38:05,104.007,0x0187,300,10,0x0081,0,65535,65535,1,26.1,12578,1143,1201,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15832,-15832,-18848,-18848,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4194,4189,0,12571,12673,1115,1126,1116,0,468,472,467,0,1433,1505,29.7,25.3,26.1,25.9,196.3,26.1,-273.2,25.7,6426,6854,6276,6670,6550,6426,6854,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,344,576,512,576,0,-193,-237,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-193,1,0.42,4065,576,512,576,0,282,1040,0,0,576,512,576,0,16384,5836,5924,1133,SUCCESS 27,2021-05-05 22:38:09,108.007,0x0187,300,10,0x0081,0,65535,65535,1,26.1,12576,1125,1184,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15832,-15832,-18848,-18848,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4191,4194,4189,0,12571,12673,1102,1115,1117,0,462,468,468,0,1412,1484,29.7,25.3,26.1,26.0,196.3,26.1,-273.2,25.7,6427,6856,6276,6670,6551,6427,6856,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,348,576,512,576,0,-194,-239,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-194,1,0.42,4065,576,512,576,0,282,1036,0,0,576,512,576,0,16384,5836,5924,1126,SUCCESS 28,2021-05-05 22:38:13,112.008,0x0187,300,10,0x0081,0,65535,65535,1,26.1,12577,1114,1169,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15853,-15853,-18873,-18873,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4195,4189,0,12571,12672,1097,1096,1100,0,460,460,461,0,1399,1465,29.8,25.3,26.1,26.0,196.7,26.1,-273.2,25.8,6428,6857,6276,6670,6552,6428,6857,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,352,576,512,576,0,-195,-240,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-195,1,0.42,4065,576,512,576,0,282,1032,0,0,576,512,576,0,16384,5836,5924,1121,SUCCESS 29,2021-05-05 22:38:17,116.008,0x0187,300,10,0x0081,0,65535,65535,1,26.1,12576,1099,1154,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15848,-15848,-18867,-18867,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4195,4189,0,12571,12671,1082,1076,1084,0,454,451,454,0,1380,1446,29.7,25.3,26.1,26.0,196.1,26.1,-273.2,25.8,6430,6859,6276,6670,6554,6430,6859,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,356,576,512,576,0,-197,-242,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-197,1,0.42,4065,576,512,576,0,282,1028,0,0,576,512,576,0,16384,5836,5924,1131,SUCCESS 30,2021-05-05 22:38:21,120.008,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12576,1087,1139,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15856,-15856,-18876,-18876,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4194,4189,0,12569,12673,1077,1076,1056,0,451,451,442,0,1367,1428,29.8,25.3,26.2,26.0,196.1,26.2,-273.2,25.8,6431,6861,6276,6670,6555,6431,6861,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,360,576,512,576,0,-198,-244,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-198,1,0.42,4065,576,512,576,0,282,1024,0,0,576,512,576,0,16384,5836,5924,1122,SUCCESS 31,2021-05-05 22:38:25,124.008,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12577,1077,1126,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15860,-15860,-18881,-18881,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4194,4189,0,12572,12673,1056,1049,1052,0,443,440,441,0,1349,1411,29.7,25.3,26.2,26.0,196.3,26.2,-273.2,25.8,6432,6862,6276,6670,6556,6432,6862,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,364,576,512,576,0,-199,-245,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-199,1,0.42,4065,576,512,576,0,282,1020,0,0,576,512,576,0,16384,5836,5924,1118,SUCCESS 32,2021-05-05 22:38:29,128.008,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12576,1066,1112,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15864,-15864,-18886,-18886,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4195,4190,0,12572,12671,1062,1049,1058,0,445,440,443,0,1338,1395,29.7,25.3,26.2,25.9,196.1,26.2,-273.2,25.8,6433,6863,6276,6670,6557,6433,6863,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,368,576,512,576,0,-200,-246,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-200,1,0.42,4065,576,512,576,0,282,1016,0,0,576,512,576,0,16384,5836,5924,1173,SUCCESS 33,2021-05-05 22:38:33,132.009,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12576,1050,1099,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15864,-15864,-18886,-18886,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4194,4189,0,12570,12673,1032,1036,1027,0,433,434,430,0,1315,1378,29.8,25.3,26.2,25.9,196.0,26.2,-273.2,25.8,6434,6864,6276,6670,6558,6434,6864,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,372,576,512,576,0,-201,-247,1,416,0,472,0,6589,6610,6757,0,0,0,0,0,-201,1,0.42,4065,576,512,576,0,282,1012,0,0,576,512,576,0,16384,5836,5924,1102,SUCCESS 34,2021-05-05 22:38:37,136.010,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12577,1039,1086,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15872,-15872,-18895,-18895,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4195,4190,0,12572,12673,1018,1027,1022,0,427,431,428,0,1304,1362,29.7,25.3,26.2,25.9,196.1,26.2,-273.2,25.8,6436,6867,6276,6670,6560,6436,6867,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,376,576,512,576,0,-203,-250,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-203,2,0.42,4065,576,512,576,0,282,1008,0,0,576,512,576,0,16384,5836,5924,1144,SUCCESS 35,2021-05-05 22:38:41,140.009,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12577,1034,1074,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15876,-15876,-18900,-18900,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4195,4190,0,12572,12672,1020,1017,1007,0,428,427,422,0,1298,1347,29.8,25.3,26.2,25.9,196.7,26.2,-273.2,25.8,6437,6868,6276,6670,6561,6437,6868,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,380,576,512,576,0,-204,-251,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-204,2,0.42,4065,576,512,576,0,282,1004,0,0,576,512,576,0,16384,5836,5924,1136,SUCCESS 36,2021-05-05 22:38:45,144.009,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12578,1020,1063,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15884,-15884,-18910,-18910,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4195,4190,0,12571,12673,1003,1010,1012,0,420,424,424,0,1283,1333,29.7,25.3,26.2,25.9,196.3,26.2,-273.2,25.8,6438,6869,6276,6670,6562,6438,6869,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,384,576,512,576,0,-205,-252,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-205,2,0.42,4065,576,512,576,0,282,1000,0,0,576,512,576,0,16384,5836,5924,1130,SUCCESS 37,2021-05-05 22:38:49,148.010,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12577,1011,1052,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15879,-15879,-18904,-18904,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4195,4190,0,12572,12673,1004,994,1006,0,421,417,422,0,1270,1319,29.8,25.3,26.2,26.0,196.1,26.2,-273.2,25.8,6439,6870,6276,6670,6563,6439,6870,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,388,576,512,576,0,-206,-253,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-206,2,0.42,4065,576,512,576,0,282,996,0,0,576,512,576,0,16384,5836,5924,1154,SUCCESS 38,2021-05-05 22:38:53,152.010,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12578,1003,1041,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15884,-15884,-18910,-18910,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4195,4190,0,12572,12673,992,995,1009,0,416,417,423,0,1263,1306,29.8,25.3,26.2,26.0,196.3,26.2,-273.2,25.8,6440,6872,6276,6670,6564,6440,6872,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,392,576,512,576,0,-207,-255,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-207,2,0.42,4065,576,512,576,0,282,992,0,0,576,512,576,0,16384,5836,5924,1101,SUCCESS 39,2021-05-05 22:38:57,156.010,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12577,996,1031,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15888,-15888,-18914,-18914,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4196,4190,0,12572,12673,984,989,988,0,412,415,414,0,1252,1294,29.7,25.3,26.2,25.9,196.1,26.2,-273.2,25.8,6441,6873,6276,6670,6565,6441,6873,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,396,576,512,576,0,-208,-256,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-208,2,0.42,4065,576,512,576,0,282,988,0,0,576,512,576,0,16384,5836,5924,1157,SUCCESS 40,2021-05-05 22:39:01,160.010,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12578,990,1022,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15888,-15888,-18914,-18914,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4196,4190,0,12572,12673,988,977,978,0,414,410,410,0,1245,1282,29.8,25.3,26.2,26.0,196.3,26.2,-273.2,25.8,6442,6874,6276,6670,6566,6442,6874,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,400,576,512,576,0,-209,-257,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-209,2,0.42,4065,576,512,576,0,282,984,0,0,576,512,576,0,16384,5836,5924,1151,SUCCESS 41,2021-05-05 22:39:05,164.011,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12579,977,1013,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15891,-15891,-18918,-18918,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4191,4195,4190,0,12573,12672,953,969,958,0,399,406,401,0,1230,1271,29.8,25.3,26.2,26.0,196.1,26.2,-273.2,25.8,6443,6875,6276,6670,6567,6443,6875,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,404,576,512,576,0,-210,-258,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-210,2,0.42,4065,576,512,576,0,282,980,0,0,576,512,576,0,16384,5836,5924,1144,SUCCESS 42,2021-05-05 22:39:09,168.011,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12579,969,1003,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15891,-15891,-18918,-18918,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4195,4189,0,12572,12673,967,949,963,0,405,398,403,0,1216,1259,29.8,25.3,26.2,26.0,196.0,26.2,-273.2,25.8,6445,6878,6276,6670,6568,6445,6878,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,408,576,512,576,0,-212,-261,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-212,2,0.42,4065,576,512,576,0,282,976,0,0,576,512,576,0,16384,5836,5924,1105,SUCCESS 43,2021-05-05 22:39:13,172.011,0x0187,300,10,0x0081,0,65535,65535,1,26.2,12580,959,994,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15891,-15891,-18918,-18918,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4195,4190,0,12574,12673,969,944,956,0,406,396,401,0,1206,1247,29.8,25.3,26.2,26.0,196.3,26.2,-273.2,25.8,6446,6879,6276,6670,6570,6446,6879,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,412,576,512,576,0,-213,-262,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-213,2,0.42,4065,576,512,576,0,282,972,0,0,576,512,576,0,16384,5836,5924,1099,SUCCESS 44,2021-05-05 22:39:17,176.011,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12578,951,984,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15895,-15895,-18923,-18923,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4196,4191,0,12574,12673,934,929,939,0,392,390,394,0,1194,1235,29.8,25.3,26.2,26.0,196.1,26.2,-273.2,25.8,6447,6880,6276,6670,6571,6447,6880,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,416,576,512,576,0,-214,-263,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-214,2,0.42,4065,576,512,576,0,282,968,0,0,576,512,576,0,16384,5836,5924,1156,SUCCESS 45,2021-05-05 22:39:21,180.011,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12579,941,975,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15900,-15900,-18929,-18929,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4196,4190,0,12572,12674,940,929,931,0,394,390,390,0,1184,1223,29.8,25.3,26.2,26.0,196.1,26.2,-273.2,25.8,6448,6882,6276,6670,6572,6448,6882,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,420,576,512,576,0,-215,-265,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-215,2,0.42,4065,576,512,576,0,282,964,0,0,576,512,576,0,16384,5836,5924,1197,SUCCESS 46,2021-05-05 22:39:25,184.012,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12578,934,966,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15900,-15900,-18929,-18929,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4191,4196,4190,0,12573,12674,937,928,923,0,393,389,387,0,1173,1212,29.8,25.3,26.2,26.0,196.1,26.3,-273.2,25.8,6449,6883,6276,6670,6573,6449,6883,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,424,576,512,576,0,-216,-266,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-216,2,0.42,4065,576,512,576,0,282,960,0,0,576,512,576,0,16384,5836,5924,1110,SUCCESS 47,2021-05-05 22:39:29,188.012,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12579,927,958,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15900,-15900,-18929,-18929,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4196,4190,0,12574,12674,922,914,918,0,387,384,385,0,1164,1202,29.7,25.3,26.3,26.0,196.3,26.3,-273.2,25.8,6450,6884,6276,6670,6574,6450,6884,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,428,576,512,576,0,-217,-267,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-217,2,0.42,4065,576,512,576,0,282,956,0,0,576,512,576,0,16384,5836,5924,1104,SUCCESS 48,2021-05-05 22:39:33,192.012,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12579,922,950,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15903,-15903,-18932,-18932,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4196,4191,0,12574,12674,913,907,910,0,383,381,381,0,1157,1192,29.8,25.3,26.3,26.0,196.3,26.3,-273.2,25.8,6451,6885,6276,6670,6575,6451,6885,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,432,576,512,576,0,-218,-268,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-218,2,0.42,4065,576,512,576,0,282,952,0,0,576,512,576,0,16384,5836,5924,1130,SUCCESS 49,2021-05-05 22:39:37,196.012,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12579,915,942,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15907,-15907,-18937,-18937,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4196,4191,0,12574,12674,905,909,910,0,379,381,381,0,1151,1183,29.8,25.3,26.3,26.0,195.6,26.3,-273.2,25.8,6452,6886,6276,6670,6576,6452,6886,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,436,576,512,576,0,-219,-269,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-219,2,0.42,4065,576,512,576,0,282,948,0,0,576,512,576,0,16384,5836,5924,1154,SUCCESS 50,2021-05-05 22:39:41,200.013,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12580,909,935,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15911,-15911,-18942,-18942,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4196,4190,0,12575,12674,898,893,905,0,377,375,379,0,1141,1173,29.7,25.3,26.3,26.0,196.3,26.3,-273.2,25.8,6453,6888,6276,6670,6577,6453,6888,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,440,576,512,576,0,-220,-271,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-220,2,0.42,4065,576,512,576,0,282,944,0,0,576,512,576,0,16384,5836,5924,1147,SUCCESS 51,2021-05-05 22:39:45,204.013,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12580,900,927,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15911,-15911,-18942,-18942,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4197,4190,0,12574,12675,888,894,894,0,372,375,375,0,1130,1164,29.8,25.3,26.3,26.0,196.1,26.3,-273.2,25.8,6454,6889,6276,6670,6578,6454,6889,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,444,576,512,576,0,-221,-272,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-221,2,0.42,4065,576,512,576,0,282,940,0,0,576,512,576,0,16384,5836,5924,1108,SUCCESS 52,2021-05-05 22:39:49,208.013,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12580,893,920,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15911,-15911,-18942,-18942,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4196,4190,0,12574,12676,887,881,883,0,372,370,370,0,1122,1155,29.8,25.3,26.3,26.0,196.3,26.3,-273.2,25.8,6455,6890,6276,6670,6579,6455,6890,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,448,576,512,576,0,-222,-273,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-222,2,0.42,4065,576,512,576,0,282,936,0,0,576,512,576,0,16384,5836,5924,1071,SUCCESS 53,2021-05-05 22:39:53,212.013,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12581,886,912,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15915,-15915,-18946,-18946,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4196,4191,0,12574,12675,877,869,879,0,368,365,368,0,1112,1145,29.7,25.3,26.3,26.0,196.1,26.3,-273.2,25.8,6456,6891,6276,6670,6580,6456,6891,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,452,576,512,576,0,-223,-274,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-223,2,0.42,4065,576,512,576,0,282,932,0,0,576,512,576,0,16384,5836,5924,1081,SUCCESS 54,2021-05-05 22:39:57,216.014,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12582,879,905,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15915,-15915,-18946,-18946,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4198,4191,0,12575,12676,870,874,872,0,365,367,365,0,1104,1136,29.8,25.3,26.3,26.0,196.1,26.3,-273.2,25.8,6457,6893,6276,6670,6581,6457,6893,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,456,576,512,576,0,-224,-276,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-224,2,0.42,4065,576,512,576,0,282,928,0,0,576,512,576,0,16384,5836,5924,1231,SUCCESS 55,2021-05-05 22:40:01,220.014,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12582,872,898,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15919,-15919,-18951,-18951,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4197,4191,0,12574,12674,864,865,858,0,362,363,360,0,1094,1127,29.8,25.3,26.3,26.0,196.1,26.3,-273.2,25.8,6458,6894,6276,6670,6582,6458,6894,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,460,576,512,576,0,-225,-277,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-225,2,0.42,4065,576,512,576,0,282,924,0,0,576,512,576,0,16384,5836,5924,1098,SUCCESS 56,2021-05-05 22:40:05,224.014,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12582,867,891,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15919,-15919,-18951,-18951,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4197,4191,0,12574,12676,852,849,851,0,357,356,357,0,1088,1118,29.7,25.3,26.3,26.1,196.1,26.3,-273.2,25.9,6459,6895,6276,6670,6583,6459,6895,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,464,576,512,576,0,-226,-278,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-226,2,0.42,4065,576,512,576,0,282,920,0,0,576,512,576,0,16384,5836,5924,1107,SUCCESS 57,2021-05-05 22:40:09,228.014,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12582,859,884,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15919,-15919,-18951,-18951,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4197,4192,0,12577,12678,854,850,856,0,358,357,359,0,1080,1110,29.8,25.3,26.3,26.1,196.3,26.3,-273.2,25.9,6460,6896,6276,6670,6584,6460,6896,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,468,576,512,576,0,-227,-279,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-227,2,0.42,4065,576,512,576,0,282,916,0,0,576,512,576,0,16384,5836,5924,1178,SUCCESS 58,2021-05-05 22:40:13,232.014,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12583,852,877,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15923,-15923,-18956,-18956,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4197,4191,0,12574,12677,841,872,880,0,353,366,369,0,1076,1102,29.8,25.3,26.3,26.1,196.1,26.3,-273.2,25.9,6461,6898,6276,6670,6585,6461,6898,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,472,576,512,576,0,-228,-281,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-228,2,0.42,4065,576,512,576,0,282,912,0,0,576,512,576,0,16384,5836,5924,1128,SUCCESS 59,2021-05-05 22:40:17,236.015,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12582,848,871,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15923,-15923,-18956,-18956,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4195,4197,4191,0,12577,12678,862,878,881,0,362,368,369,0,1081,1095,29.8,25.3,26.3,26.1,197.8,26.3,-273.2,25.9,6462,6899,6276,6670,6586,6462,6899,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,476,576,512,576,0,-229,-282,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-229,2,0.42,4065,576,512,576,0,282,908,0,0,576,512,576,0,16384,5836,5924,1102,SUCCESS 60,2021-05-05 22:40:21,240.015,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12583,875,872,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15923,-15923,-18956,-18956,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4195,4201,4193,0,12577,12679,855,863,869,0,359,363,364,0,1100,1097,29.8,25.3,26.3,26.1,196.1,26.3,-273.2,25.9,6463,6900,6276,6670,6587,6463,6900,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,480,576,512,576,0,-230,-283,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-230,2,0.42,4065,576,512,576,0,282,904,0,0,576,512,576,0,16384,5836,5924,1112,SUCCESS 61,2021-05-05 22:40:25,244.015,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12585,850,865,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15926,-15926,-18960,-18960,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4198,4191,0,12578,12676,825,821,828,0,346,345,347,0,1057,1087,29.7,25.3,26.3,26.1,196.3,26.3,-273.2,25.9,6463,6900,6276,6670,6587,6463,6900,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,484,576,512,576,0,-230,-283,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-231,2,0.42,4065,576,512,576,0,282,900,0,0,576,512,576,0,16384,5836,5924,1152,SUCCESS 62,2021-05-05 22:40:29,248.015,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12582,825,857,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15931,-15931,-18965,-18965,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4198,4192,0,12577,12677,815,820,830,0,342,344,348,0,1037,1076,29.7,25.3,26.3,26.1,196.4,26.3,-273.2,25.9,6464,6901,6276,6670,6588,6464,6901,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,488,576,512,576,0,-231,-284,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-231,2,0.42,4065,576,512,576,0,282,896,0,0,576,512,576,0,16384,5836,5924,1131,SUCCESS 63,2021-05-05 22:40:33,252.016,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12582,817,848,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15931,-15931,-18965,-18965,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4198,4194,0,12577,12679,818,805,817,0,343,338,343,0,1025,1065,29.7,25.3,26.3,26.1,196.1,26.3,-273.2,25.9,6465,6902,6276,6670,6589,6465,6902,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,492,576,512,576,0,-232,-285,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-232,2,0.42,4065,576,512,576,0,282,892,0,0,576,512,576,0,16384,5836,5924,1125,SUCCESS 64,2021-05-05 22:40:37,256.016,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12583,811,840,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15935,-15935,-18970,-18970,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4198,4192,0,12579,12676,811,812,810,0,340,341,340,0,1019,1055,29.7,25.3,26.3,26.1,196.1,26.3,-273.2,25.9,6466,6904,6276,6670,6590,6466,6904,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,496,576,512,576,0,-233,-287,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-233,2,0.42,4065,576,512,576,0,282,888,0,0,576,512,576,0,16384,5836,5924,1133,SUCCESS 65,2021-05-05 22:40:41,260.016,0x0187,300,10,0x0081,0,65535,65535,1,26.3,12584,807,833,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15935,-15935,-18970,-18970,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4195,4198,4192,0,12577,12678,824,804,803,0,346,338,337,0,1012,1045,29.8,25.3,26.4,26.1,196.5,26.4,-273.2,25.9,6467,6905,6276,6670,6591,6467,6905,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,500,576,512,576,0,-234,-288,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-234,2,0.42,4065,576,512,576,0,282,884,0,0,576,512,576,0,16384,5836,5924,1110,SUCCESS 66,2021-05-05 22:40:45,264.016,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12584,803,826,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15935,-15935,-18970,-18970,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4199,4192,0,12577,12678,797,787,795,0,334,330,333,0,1009,1037,29.7,25.3,26.3,26.2,196.1,26.3,-273.2,25.9,6468,6906,6276,6670,6592,6468,6906,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,504,576,512,576,0,-235,-289,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-235,2,0.42,4065,576,512,576,0,282,880,0,0,576,512,576,0,16384,5836,5924,1166,SUCCESS 67,2021-05-05 22:40:49,268.016,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12583,798,820,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4198,4192,0,12578,12677,802,792,786,0,336,332,329,0,999,1029,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,25.9,6469,6907,6276,6670,6593,6469,6907,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,508,576,512,576,0,-236,-290,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-236,2,0.42,4065,576,512,576,0,282,876,0,0,576,512,576,0,16384,5836,5924,1240,SUCCESS 68,2021-05-05 22:40:53,272.017,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12583,794,814,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4199,4192,0,12577,12678,785,793,788,0,329,333,330,0,995,1022,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,25.9,6470,6909,6276,6670,6594,6470,6909,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,512,576,512,576,0,-237,-292,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-237,2,0.42,4065,576,512,576,0,282,872,0,0,576,512,576,0,16384,5836,5924,1090,SUCCESS 69,2021-05-05 22:40:57,276.018,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12585,789,808,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4199,4193,0,12577,12678,782,778,795,0,328,327,333,0,991,1015,29.7,25.3,26.4,26.2,196.5,26.4,-273.2,25.9,6471,6910,6276,6670,6595,6471,6910,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,516,576,512,576,0,-238,-293,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-238,2,0.42,4065,576,512,576,0,282,868,0,0,576,512,576,0,16384,5836,5924,1130,SUCCESS 70,2021-05-05 22:41:01,280.017,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12584,783,803,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4195,4198,4192,0,12579,12679,771,779,788,0,323,327,330,0,988,1008,29.7,25.3,26.4,26.2,195.6,26.4,-273.2,25.9,6472,6911,6276,6670,6595,6472,6911,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,520,576,512,576,0,-239,-294,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-239,2,0.42,4065,576,512,576,0,282,864,0,0,576,512,576,0,16384,5836,5924,1141,SUCCESS 71,2021-05-05 22:41:05,284.017,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12585,777,797,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4199,4193,0,12580,12676,765,772,774,0,321,324,325,0,978,1002,29.7,25.3,26.4,26.2,196.1,26.4,-273.2,25.9,6472,6911,6276,6670,6596,6472,6911,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,524,576,512,576,0,-239,-294,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-239,2,0.42,4065,576,512,576,0,282,860,0,0,576,512,576,0,16384,5836,5924,1180,SUCCESS 72,2021-05-05 22:41:09,288.018,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12584,772,792,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4199,4195,0,12577,12679,766,772,764,0,321,324,320,0,970,995,29.7,25.3,26.4,26.2,196.1,26.4,-273.2,25.9,6473,6912,6276,6670,6597,6473,6912,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,528,576,512,576,0,-240,-295,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-240,2,0.42,4065,576,512,576,0,282,856,0,0,576,512,576,0,16384,5836,5924,1142,SUCCESS 73,2021-05-05 22:41:13,292.018,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12584,767,787,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4195,4199,4193,0,12579,12679,755,773,749,0,317,325,314,0,964,988,29.7,25.3,26.4,26.2,196.5,26.4,-273.2,25.9,6474,6914,6276,6670,6598,6474,6914,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,532,576,512,576,0,-241,-297,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-241,2,0.42,4065,576,512,576,0,282,852,0,0,576,512,576,0,16384,5836,5924,1119,SUCCESS 74,2021-05-05 22:41:17,296.018,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12584,764,781,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4194,4200,4192,0,12580,12679,752,763,742,0,315,320,311,0,960,981,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,25.9,6475,6915,6276,6670,6599,6475,6915,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,536,576,512,576,0,-242,-298,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-242,2,0.42,4065,576,512,576,0,282,848,0,0,576,512,576,0,16384,5836,5924,1128,SUCCESS 75,2021-05-05 22:41:21,300.018,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12584,757,776,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4196,4200,4194,0,12579,12680,749,740,741,0,314,311,311,0,949,975,29.7,25.4,26.4,26.2,196.3,26.4,-273.2,25.9,6476,6916,6276,6670,6600,6476,6916,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,540,576,512,576,0,-243,-299,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-243,2,0.42,4065,576,512,576,0,282,844,0,0,576,512,576,0,16384,5836,5924,1154,SUCCESS 76,2021-05-05 22:41:25,304.019,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12585,751,770,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4195,4199,4193,0,12580,12679,744,743,747,0,312,312,313,0,943,968,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,25.9,6477,6917,6276,6670,6601,6477,6917,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,544,576,512,576,0,-244,-300,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-244,2,0.42,4065,576,512,576,0,282,840,0,0,576,512,576,0,16384,5836,5924,1132,SUCCESS 77,2021-05-05 22:41:29,308.019,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12585,751,765,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4199,4193,0,12580,12679,739,745,728,0,310,313,305,0,943,962,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,26.0,6477,6917,6276,6670,6601,6477,6917,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,548,576,512,576,0,-245,-301,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-245,2,0.42,4065,576,512,576,0,282,836,0,0,576,512,576,0,16384,5836,5924,1124,SUCCESS 78,2021-05-05 22:41:33,312.019,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12586,748,761,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4196,4201,4194,0,12580,12683,738,743,730,0,310,312,306,0,939,957,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,25.9,6478,6918,6276,6670,6602,6478,6918,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,552,576,512,576,0,-245,-301,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-245,2,0.42,4065,576,512,576,0,282,832,0,0,576,512,576,0,16384,5836,5924,1086,SUCCESS 79,2021-05-05 22:41:37,316.019,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12585,734,756,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4196,4201,4195,0,12582,12679,717,710,726,0,301,298,305,0,923,949,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,25.9,6479,6920,6276,6670,6603,6479,6920,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,556,576,512,576,0,-246,-303,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-246,2,0.42,4065,576,512,576,0,282,828,0,0,576,512,576,0,16384,5836,5924,1145,SUCCESS 80,2021-05-05 22:41:41,320.019,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12563,0,626,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4186,4193,4185,0,12557,12652,0,0,0,0,0,0,0,0,0,735,29.7,25.3,26.4,26.2,196.1,26.4,-273.2,26.0,6479,6920,6276,6670,6603,6479,6920,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,560,576,512,576,0,-246,-303,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-246,2,0.42,4065,576,512,576,0,282,824,0,0,576,512,576,0,16384,5836,5924,1153,SUCCESS 81,2021-05-05 22:41:45,324.020,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12560,0,475,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4184,4193,4184,0,12556,12651,0,0,0,0,0,0,0,0,0,558,29.7,25.3,26.4,26.2,196.3,26.4,-273.2,25.9,6479,6920,6276,6670,6603,6479,6920,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,564,576,512,576,0,-246,-303,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-246,2,0.42,4065,576,512,576,0,282,820,0,0,576,512,576,0,16384,5836,5924,1115,SUCCESS 82,2021-05-05 22:41:49,328.020,0x0187,300,10,0x0081,0,65535,65535,1,26.4,12559,0,361,101,99,38,6213,6276,65535,65535,0,3800,12600,0x0080,0,-15938,-15938,-18974,-18974,35,0x0187,0x1000,0x10,0x0008,0x90,0x0014,0x0018,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4183,4192,4184,0,12555,12648,0,0,0,0,0,0,0,0,0,424,29.6,25.4,26.4,26.2,194.8,26.4,-273.2,26.0,6479,6920,6276,6670,6603,6479,6920,43,53,6276,6670,24.6,24.3,1000,1000,1000,0,0,0,0,0,0,14,0,0,0,0,568,576,512,576,0,-246,-303,2,416,0,472,0,6589,6610,6757,0,0,0,0,0,-246,2,0.42,4065,576,512,576,0,282,816,0,0,576,512,576,0,16384,5836,5924,1107,SUCCESS