Hello, TI expert.
I am testing the LLC block by applying UCC25600, TL103WAIDR.
Spec is shown in the table below. (Max 360V / 3A output)
There is a situation where CC/CV control is not possible during LLC operation, so it is during debugging but cannot be resolved.
So, I want to check whether the current LLC circuit is suitable for satisfying the output specifications.
Please check if the attached LLC circuit diagram can implement the output specifications.
Please tell us if there is a part where you need to modify the inductance, resonance cap, and circuit diagram RC values to satisfy the corresponding output specifications.
The current LLC specifications are as follows:
1) Lp(1st inductance)
Trans(T302, T303) : 36uH (In the circuit diagram, two transformers are connected in series, Lp: 72uH)
2) Lr(Leakage inductance) :
Trans(T302, T303): 7uH (In the circuit diagram, two transformers are connected in series, Lr: 14uH)
Leakage Trans(T301) : 10uH
3) Number of turns
Trans(T302, T303) : 1st 11turns / 2nd 30turns (In the circuit diagram, the first is 22 turns in series and the second is 30 turns in parallel.)
4) Resonance cap : 94nF
Thank you.
(LLC)_Charger_SCH_REV01_210510.pdf