Other Parts Discussed in Thread: BQSTUDIO
Hello,
We ran a learning cycle using datasheet settings (successfull), But our application settings are different. We wrote the application settings after doing the learning cycle.
Application:
- Charge voltage=57.6V
- Term voltage=46.8V
Datasheet settings:
- charge voltage=58.4V
- Term voltage=40V
What could be the consequences?
- The grid point never exceed 12, is that the reason?
- when doing a full discharge with High rate (using application voltage as term voltage), We have 5% SOC remaining. After a long relax period, Soc changes from 5% to 0
I Can't see any sign of good accuracy in this, could you advise me?
thanks,
yf