Other Parts Discussed in Thread: ASH, LM74700-Q1
Hi All,
We have an existing application that uses a TPS25982 as a standard E-Fuse and were wondering if was possible use two of these IC's as a priority muxing system like in:
It is a simple application that feeds into a regulated system.
The requirements are:
- Main Input 11V - 17V DC Supply
- Aux Input 11V - 17V Battery Supply
- Output of 11V - 17V at 8A - 12A
- Ability to be used for hotswap and E-fuse to consolidate the amount of different components we have to have on hand
We understand that this application may require an external O-Ring diode so we are open to using a different component overall.
Thanks!