This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2611: schematic review for -12V from 12V

Part Number: LM2611

Hi,

Could you review the schematic for -12V output from 12V?

current is 5mA.

Additionally, what component has to be changed for 50mA current?

Now R16 is 87.5kOhm.

Thanks.