This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62865: startup time

Part Number: TPS62865


Hi support team,

Is the startup time the same for the left and right ways?

It is said that the R2D converter IC takes a long time to start, but does it take time because the R2D converter is mounted even in the left way that does not use R2D?
Does it take time to detect the resistance value of the VSET/MODE pin even with any of ways?

Regards,
Dice-K

  • Hello Dice-K,

    It will take the same amount of time for the converter to startup for the Adjustable and the Fixed output voltage.

    To define if Adjustable or Fixed Output voltage is selected, an initial readout is necessary.

    As you can see in Table 8-2 of the datasheet, if a 10k Ohm resistor ( or directly linked to GND) is connected between VSET/MODE and GND. The R2D will read its value at startup and then operate in an Adjustable Output Voltage configuration.

    Let me know if you have further questions.

    Thanks a lot!

    Regards,

    Dorian