This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5036: Control to output transfer function

Part Number: LM5036

Hi team,

Do you have the uncompensated control to output transfer function and line to output transfer function for LM5036? My customer would like to have it to perform small signal model for worst case analysis.

Regards

SK Loo

  • Hi SK,

    The control to output transfer function includes the "plant" which is the power stage and is unique to your customers application use. I would recommend to ask them to download and use TI Power Stage Designer. Build the power stage using the specifications from your customer application, then click "Loop Calculator" and this will help. I like this tool because it is not connected to any specific controller but based on power topologies. SLUP340 is also helpful to use along with the "Loop Calculator." Thanks for connecting through E2E.

    Regards,

    Steve M