This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: Power management forum

Part Number: LM5117
Other Parts Discussed in Thread: LM5145

Is it possible to build a 48V to 5V/20A buck convertor using the LM5117?

  • Hello,

    We recommend the LM5145 controller for best efficiency performance at such high current - take a look at the LM5145 EVM (5V/20A/225kHz).

    Regards,

    Tim

  • Hi Tim,

    Thank you for the recommendation.  The LM5145 looks like a good match.

    A couple questions:

    1.) We have a large cap bank (500,000uF).  Will the LM5145 be able to handle the initial inrush and successfully charge this capacitance?

    2.) With the LM5117, we were hoping to use the CM output to implement a CC/CV convertor.  For example, after the initial Cap bank charge, we want to limit current from the convertor to approx. 19A. Is the LM5145 capable of performing the CC/CV function as well?

    Thanks,

    John

  • Hi John,

    See app note snva829 for CC/CV circuits. The LM5117 makes it easier as it has the CM pin. However, efficiency and thermal performance are likely critical here, hence the initial preference for the LM5145.

    In terms of startup into a very high COUT, the CC/CV circuit should manage that. Otherwise, a very high soft-start (SS) cap value is required.

    Regards,

    Tim

  • Tim,

    It looks to me like the LM5145 has OCP capability and will shut down when that limit is reached. However, it does not have the ability to operate and limit the current to some preset value below the OCP setpoint.  To do that I would have to implement a current sense resistor and feedback that voltage into the FB pin on the LM5145 as suggested in the appnote snva829. Am I correct in these assumptions?

    Is there a controller with this current limit feature already built in?  Just trying to keep things simple here...

    Thanks,

    john

  • John,

    That's correct. For constant-current (CC) operation with the LM5145, an external circuit that adjusts the current into FB is appropriate.

    The LM5117 with its CM pin provides this functionality more readily (as described int he app note mentioned above) and may be the best option for your application.

    Regards,

    Tim