Other Parts Discussed in Thread: TLV1117, LM1117, TLV767
Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with "zldo1117qgta" ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please allow us one additional business day for us to look into this for you and we will get back to you soon.
Hello Kygo,
p2p options are TLV1117 and LM1117. However, the latest device TLV767 can also compete if p2p is not required.
Regards,
Prakash L
ZLDO1117 | TLV1117 | TLV767 | LM1117 | |
AEC Q100 | NO | NO | NO | NO |
Output Options | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output |
Iout (Max) (A) | 1 | 0.8 | 1 | 0.8 |
Vin (Max) (V) | 18 | 15 | 16 | 15 |
Vin (Min) (V) | 2.7 | 2.7 | 2.5 | 2.6 |
Vout (Max) (V) | 5 | 13.7 | 14.5 | 13.8 |
Vout (Min) (V) | 1.2 | 1.25 | 0.8 | 1.25 |
Fixed Output Options (V) | 1.2, 1.5, 1.8, 2.5, 3.3, 5, ADJ | 1.5, 1.8, 2.5, 3.3, 5 | 0.8, 1.8, 2.8, 3.3, 5 | 1.8, 2.5, 3.3, 5 |
Enable | NO | NO | YES | NO |
Power Good | NO | NO | NO | NO |
Output Capacitor Type | Ceramic | Non-Ceramic | Ceramic | Non-Ceramic |
PSRR @ 100KHz (dB) | 50 | 28 | 53 | 47 |
Noise (uVrms) | - | 411 | 60 | 38 |
Accuracy (%) | 2 | 3.75 | 1 | 3 |
Vdo (Typ) (mV) | 1100 | 1200 | 900 | 1200 |
Iq (Typ) (mA) | 4 | 1.7 | 0.05 | 5 |
Thermal Resistance θJA (°C/W) | 73 | 28 | 60.1 | 24 |
Min Package Area (mm2) | 22.75 | 16 | 4 | 16 |
Package Type | SOT-223, TO-252 | DDPAK/TO-263, SON, SOT-223, TO-220, TO-220, TO-252 | HVSSOP, WSON | DDPAK/TO-263, SOT-223, TO-220, TO-252, WSON |