Other Parts Discussed in Thread: TPS63060, , TPS61230A, BQ24179
I tested the part at about 1A output load, 3.5V in (1 LiIon cell) and 5V out. After EN off and on (while load stays on) the part shows only 0.2V output voltage - it does not recover the voltage. After reducing output current to below 100mA it recovers fully. Is there a possibility to achieve full recovery at high load currents (while not removing the load)? Or can you recommend another (similar small) part which does. E.g. the TPS63060 does but has not the requested performance (3V input at 5V and 1.5A output).