Hi Team,
We have received an inquiry from our customer as follows.
So here is what happened to BQ24610EVM. I changed the resistor R25
to 665kOhm so I can get a 16V output for charging a 14.8V battery. I
gave Vin a 19V input, and I did observed Vbat is 15.95V. However, after
I connected the battery to Vbat, I observed there is no current going in
to my battery. I measured it by connected a current meter in series
with battery and BQ24610EVM. I know the battery I used is not fully
charged, and I have tested with some other battery charger that if the
battery is charging, then there should be current flowing into the
battery. I want to know why your BQ24610EVM is not charging the
battery.
He used the default settings of the jumpers on the board.
Thank you for your support
Regards,
Danilo