Other Parts Discussed in Thread: BQSTUDIO
I've got an issue with the bq25619 lithium-ion charger and I've exhausted all self-help options. The main issue is that from a cold-start, Vsys doesn't come up when just external power is applied. It boots just fine with the battery installed but not from just external power.
Design information: Schematic attached. Design uses a removeable single-cell lithium-ion battery and has an external 5V power source. Vsys is used to power the system so I need it to come up regardless of the input source (ie: battery or external power). When just external power is applied, there is a distintive ringing on the SW output (scope plots attached showing waveform with and without external battery). I've tried doing some loading of the BAT input but I couldn't change the results. I didn't see any guidance in the datasheet regarding the need to load BAT if not battery present.
Are you able to lend any guidance before I explore other solutions?
Thanks,
Keith