Other Parts Discussed in Thread: CSD17577Q5A
Hi Guys,
Please help me to clarify to our customer about the mosfet and thermal management of CSD17312Q5.
I have posted the full inquiry of our customer below for more details:
I'm working to use a Texas Instruments mosfet (model CSD17312Q5) as a low side switch to turn a Peltier cell on and off. The electrical power consumption of the cell is high (10 Amps at 24V), but this mosfet should be able to handle it, according to the datasheet. I will definitely have to pay attention to the heating problem. This is the first time that I use a mosfet with such a large electric current (I am a beginner, I have used mosfets only for educational purposes, to turn some leds on and off), and there are some questions I would like to ask about the thermal management of the mosfet. Before choosing this model of T.E. mosfet, I looked at the datasheets of many other similar mosfets; almost all of them had in common some indications regarding the correct dissipation of heat. In particular, in order to better dissipate the heat, they suggested mounting the mosfet “on a 1-inch² (6.45-cm²), 2-oz. (0.071-mm thick) Cu pad on a 0.06-inch (1.52-mm) thick FR4 PCB ”.
In detail, it was always the pins connected to the Drain that were connected to this large copper pad, not the pins connected to the Source.
Only in a few cases have I seen some special mosfets in which above the body of the mosfet there was a small metal part connected to the Source, and a small aluminum radiator could be mounted above it, so as to also cool the Source ( as well as the Drain).
I would like to ask two questions:
1) The “1-inch², 2-oz. Cu pad ”must be exposed (as if it were a normal soldering pad) or can it be covered by the soldermask? I ask because I believe soldermask limits thermal disposal, although not as much as electrical conductivity.
2) Unfortunately, I cannot use a FR4 PCB with 2 oz of copper: I am forced to use a FR4 PCB with only 1 oz of copper. However, it is a double-layered FR4, so I can use both faces to disperse the heat, also thanks to the fact that the bottom face will still be in the air. In all the mosfets I have seen (except the special ones I mentioned a little above) it is always the pins of the Drain that take care of the heat dissipation; using both faces of a double sided FR4 PCB is it better that both faces are connected to the Drain pin, or can I connect the top face pad to the Drain pin and the bottom face pad to the Source pin? Is it useful to connect the Source pins to a copper pad to cool it down, or is it useless?
Thank you in advance for your support.
Best regards,
Jonathan