Other Parts Discussed in Thread: LM317
Hi Team,
There is good news that we DIN UA7805CKTTR
But now customer need TO-252(DPAK) package
Do we have the solution
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kygo,
UA78 | LM317 | |
AEC Q100 | NO | NO |
Output Options | Fixed Output | Adjustable Output |
Iout (Max) (A) | 1.5 | 1.5 |
Vin (Max) (V) | 38 | 40 |
Vin (Min) (V) | 7 | 3 |
Vout (Max) (V) | 24 | 37 |
Vout (Min) (V) | 5 | 1.25 |
Fixed Output Options (V) | 5, 8, 10, 12, 15, 24 | - |
Enable | NO | NO |
Power Good | NO | NO |
Output Capacitor Type | Cap Free, Non-Ceramic | Non-Ceramic |
PSRR @ 100KHz (dB) | 40 | 38 |
Noise (uVrms) | 52 | 38 |
Accuracy (%) | 3.75 | 5 |
Vdo (Typ) (mV) | 2000 | 2000 |
Iq (Typ) (mA) | 4.3 | 5 |
Thermal Resistance θJA (°C/W) | 22 | 24 |
Min Package Area (mm2) | 87.2744 | 45.5 |
Package Type | DDPAK/TO-263, TO-220, TO-220 |
DDPAK/TO-263, SOT-223, TO-252, TO-220 |
Regards,
Prakash L