Other Parts Discussed in Thread: TPS2829
Hello Team,
the TPS2819 and TPS2829 share the same datasheet and the difference is about the internal regulator.
pin 1 is NC on the TPS2829 while it is Vdd on TPS2819.
If we would use the TPS2819 instead of the TPS2829, but the PCB has pin 1 floating (it was designed for the TPS2829), thus not connected to Vcc as recommended for the TPS2819 in case Vdd is not used.
Do you see any problem by that exchange?
Can the part still work?
Considering the diode on top of the LDO, it looks that it may work, but how reliable would be?
The datasheet states that unused Vdd for the TPS2819 should be connected to Vcc, thus it will remain customer risk not connecting it.
The info above would help the risk analysis.
Thanks,
SunSet