We're confused with the LM25183 datasheet. In the Abs. maximum rating of the input pin it's 48V. But first page shows the integrated 65V MOSFET.
Is this VIN Pin able to be withstand 60Vdc value? Since safety functionality requirement, the 60VDC testing for several seconds are needed at the input voltage rail. Is LM25183 ok with this test? Very thanks.
Regards
Brian W