This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256404: minimum and maximum switching frequency in UCC256404

Part Number: UCC256404
Other Parts Discussed in Thread: UCC25600

Hello,

In my customer's desired application a tight voltage regulation is not required. Hence, I would like to restrict the upper limit of the switching frequency to enhance the efficiency at light load.  Is it possible to set the minimum and maximum switching frequency in UCC256404, similar to UCC25600?

Thank you.

Regards,

 

  • Hi, Mehdi

    It is possible to set the maximum switching frequency with UCC256404, since the maximum switching frequency is happened in burst mode. The higher burst mode threshold, the lower maximum switching frequency. You can download the excel calculation tool of UCC256404, to design the burst mode threshold based on the calculation tool.

    regarding to the minimum switching frequency, it cannot be changed, UCC256404 limit the minimum switching frequency at 35kHz.

    Yunsheng

  • Thank you, Yunsheng.

    Best,